I am testing the net-uart in contiki.
The system setup is as follow:
Contiki node: SRF06EB+CC1310EM running cc26xx-web-demo
Border router: SRF06EB+CC1310EM +BBB with running 6lbr+wrapsix
ipv6 router with ipv4: 192.168.16.1 and ipv6: bbbb::109
PC’s ipv6: bbbb::a96a:999e:b8f7:a664
PC’s ipv4: 192.168.16.11
With this setup the IBM Quickstart is working perfectly.
Now for net uart testing, I got no result so far:
Net-uart config:
remote ipv6: 0064:ff96:0000:0000:0000:0000:c0a8:100b
remote port: 55777
PC usb connected to the contiki node, and the back channel of UART is COM1, with 15200/8/N/1.
On PC, I run a serial test software which I send characters out into COM1. Meanwhile on my PC I run an UDP listener software Sokit, setting the UDP server listening port at 55777.
I suppose the contiki node receive these serial characters, then the net-uart should send UDP packet at port 55777. Meanwhile on my PC I should see UDP packet receiving in Sokit. But so far I have not succeeded.
I have also tried to put the PC’s IPV6 address to the net-uart config, the result is also not successful.
Anyone can give me clues what is problem?