Other Parts Discussed in Thread: CC2591, CC2530
Hi all,
I'm working with a Zigbee network using CC2530 + CC2591 as ZEDs, ZRTs and a ZCO.
When I configure the TX power with "MAC_MlmeSetReq(MAC_PHY_TRANSMIT_POWER,&txpower)", it looks like the configuration values on the table are backwards, because I have more TX power with a lower value.
This is the configuration code:
#ifdef HAL_PA_LNA
uint8 txpower= 0x55;
#else
uint8 txpower= 0xF5;
#endif
MAC_MlmeSetReq(MAC_PHY_TRANSMIT_POWER,&txpower);
Is this normal?
Did anyone see this behavior too?
Thanks!