I want to implement 8FSK modulation on the CC2650, are there app notes describing how this is done? I see it briefly mentioned, but looking for more information, thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to implement 8FSK modulation on the CC2650, are there app notes describing how this is done? I see it briefly mentioned, but looking for more information, thank you.
Hi Paul,
See TRM Section 23.3.3.1.2 CMD_RADIO_SETUP: Set Up Radio Settings Command Byte Index 14: 0x05: 5-Mbps coded 8-FSK.
Also, the WIKI is a good source for sample code and support: http://processors.wiki.ti.com/index.php/CC13xx_CC26xx_Tools_Overview