This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Zigbee End device trying to connect when it goes out of network. how can i disable it?

Hi All, 

I have an end device, i developed my application on sample application from the zstack 1.2.0 version (sample switch).

Here when i go out of the network my end device senses that and sending beacon requests to connect it back.

bcz of this i am facing two issues that

-> my end device is not able to join the ZO.

-> bcz of continuous beacons my end device battery is draining very fast.

i tried with zstack 1.2.2a version also. it is happening with all the end device firmware.

i want an scenario that when it goes out of the network it should search for the network and it should sense that it is out of network.

any command comes from that also fine, it wont reach my ZO.

How can i achieve this?