This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2630 / cc2650 Commissioning Cluster Support

Other Parts Discussed in Thread: CC2650, CC2630, Z-STACK, CC2530

Hello,

I need to implemet commissioning cluster into a cc2630 / cc2650 family project in an End Device, under Z-Stack HA 122a.

Is there a project I could use as a reference?

Can anybody help me on this? I know that commisioning cluster is supported for ZBA projects under cc2530 example, but how can I merge it with simpleLink cc2630 or cc2650 project? The difficulty on this is due the form of cc2650 projects that uses separate core and application projects witch they communicate using ICalls.

Also does anyone know when would an updated simplelink (including an updated TI RTOS) would be released?

Thanks in advance.


Spiros