Hello
I am working with Z-Stack Home 1.2.1, I have 15 - 20 total zigbee routers (CC2530), and beaglebone black with CC2531 dongle as coordinator.
My problem is I cannot add more than 9 routers in my network.
I have previously observed this problem with maximum 6 routers. And also with maximum 11 routers.
Please help me with following queries:
1) What is the parameter in Coordinator that decides maximum number of routers that can be joined in the network?
2) I have always used the precompiled binary for CC2531 dongle provided with Linux gateway 1.0.1.. If I want to change that parameter in coordinator code, what steps should I follow
3) As far as I have observed, the maximum number of routers is not always same, I have to add and check how many routers can be added. Why is this so?
Please help urgently