Other Parts Discussed in Thread: CC2531, CC2650
I use RPI + CC2531 USB Dongle and sensortag cc2650 to perform a sensor network. And I am testing the power consumption of cc2650.
sensortag is running web-demo to send data to IBM cloud.
And the power consumption is basically the same as here: https://github.com/contiki-os/contiki/issues/1305%C2%A0
If cc26xx-web-demo is functioning properly (can publish MQTT message and display sensor reading on the IBM web dashboard) the current consumption is about 3mA when publishing and 0.47mA when NOT publishing.
I find that the current is sometimes up to 9 mA which is explained in the link above: If I turned off wrapsix NAT64 program running on the Boarder Router, the current shoot up to 8mAwhile LED keeps on. But the thing is I didn't turn off wrapsix NAT64 manually.
So I think wrapsix itself is not stable. Have any of you encountered this? How to solve this?
Thank you.
Best wishes,
Tiancong Gu