This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC26xx or CC13xx for 80 m RF range application?

Hi,

I have an outdoor application (can be used indoor as well) that should have max. 80m range. I designed a HW based on CC26xx module, but my modules' RF performance is not reliable after 15m. 

I did test with CC2650EM + SmartRF. In general it seems it operates fine. Although, PER is not stable. I know channel parameters change, but I couldn't judge if C26xx is good for 80m range application or would you recommend to use cc13xx instead?

I am in more favor of CC26xx since all my hardware and edge router etc. are designed for 2.45 GHz and ready to operate.

Could you please share your CC26xx range experience?