Hi All,
I am working on flashing CC2530 through TI's AM57xx host processor.
When I start flashing CC2530, first we put the chip into debug mode. I can see two falling-edge transitions on pin debug clock, while the
RESET_N input is held low and than RESET_N pin to high. Even after that I feel that CC2530 is not going into Debug mode, because when we give any command to Chip after putting it to DEBUG mode, it does not respond back.
Are there any timing sequence we need to follow to put CC2530 into debug mode?
Please suggest some solutions. I need help barely.
Thanks,
Krinali Shah