Other Parts Discussed in Thread: CC2538, Z-STACK
Hi,
For CC2538, how can I change the default PANID and channel setting.
I am using
"
uint32 MyChannel=0x80000;
uint8 status;
status=osal_nv_write(ZCD_NV_CHANLIST, 0, sizeof(MyChannel) , &MyChannel);
uint16 myPANID = 0xF78A;
status=osal_nv_write(ZCD_NV_PANID, 0, sizeof( myPANID ), &myPANID );
"
But both status return "10", i.e. NV_OPER_FAILED. I have called osal_nv_init before calling write function.
One more question about this "osal_nv_item_len( ZCD_NV_CHANLIST )", it is always 0.
Thanks.