Other Parts Discussed in Thread: CC2538, CC2531, CC2530
Hai all,
I have 10 cc2538 modules.i created zigbee mesh network. Here i have small confusion mesh have the self routing property and hop to hop Acks.
But my network shows different behavior.
1.CC2531(coordinator),remain boards are routers and few end devices.End node send temperature data to nearest router(0x1254) {single hope,source and dest}
and i got Ack from MAC layer.
2.Destination end point is (0x1425),but in between routers nearly 7 all are board cast to all.what is this means .
3.Is this the real mesh network.because mesh should have single route.but here all routers are acts as a repeaters.So i cant calculate efficiency of the network .
please help me out this issue.