This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Setup a basic Sensory network using Zigbee

Hi Guys,

I'm quite new to Zigbee and was wondering how I go about constructing a basic Sensory mesh network using Zigbee.

What I was after, was to have a number of Zigbee sensor nodes (which are physically connected to a sensor) that will alert once an input has been detected. These inputs can then be transferred to a Zigbee coordinator that can notify the affected user (via an SMS) about the location of detection found by the sensor.

Is this possible to be constructed using TI hardware/software?

You're help will be greatly appreciated,

Kind Regards,

Youf