Hai Guys...
Iam quite new with Z-stack and CC2520 development environment. Here is my application Overview,
I need to do the following:
1) Setup a timer for every 7 ms.
2) After 7 ms the program should sample values from ADC.
3) When 100 samples of ADC are collected, the program should send them to Coordinator.
4) Coordinator should send these values to PC via serial link.
5) We need a small program on PC that should collect the samples sent from coordinator via serial link and save it in a file. This is just like ZSensorMonitor Program. Can we get the source code of Zsensor monitor program somhow?
Can anybody help me in getting my application executed...
Regards
Nayeem Sk