Other Parts Discussed in Thread: CC2531, CC2592, CC2630, CC2650, CC2530
Hi,all,
I'm using smartRF studio 7 (V2.4.3) to get the rssi of our modules .
the results of the testing as following:
-------------------------------------------------------------------------------------------------------------------------------------
mudules(TX) | packet sniffer (cc2531) | smartRF studio 7(launchpad 2650 as receiver.)
-------------------------------------------------------------------------------------------------------------------------------------
CC2630 + CC2592 | +11dbm | -4 dbm
------------------------------------------------------------------------------------------------------------------------------------
CC2650 launchpad | -5dbm | -4 dbm
-------------------------------------------------------------------------------------------------------------------------------------
the MAX rssi of the smartRF studio seems to be limited .
i had used the smartRF studio get the correct RSSI of CC2530 + RFX2401 two years ago.
what happened?
______________________________________________________________________________
//2016.11.18
the max rssi cc2530 + rxf2401 in the packet sniffer (cc2531) is +3dbm, i don't get larger.
if i want to get the correct value ,how to do it?
Is the value of rssi register needed to convert using the macRadioDefsTxPwrCC2592[] table?