This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Config GPIO / ADC for CC2530 GenericApp



Hi everyone,

1) I configured pin P0_6 and P0_7 as below

P0SEL &=(~BV(6));
P0DIR |= BV(6);

P0SEL &=(~BV(7));
P0DIR |= BV(7);

It's working OK but sometime I set P0_6 = 1 but It's still 0 ( I measured by VOM)

How can I check the ouput P0_6 after set to 1?

2) Besides, I used P0_5 as ADC input.

Set HAL_ADC=TRUE in Preprocessor and

HalAdcSetReference(HAL_ADC_REF_125V);

adc_ain5=HalAdcRead(HAL_ADC_CHN_AIN5,HAL_ADC_RESOLUTION_12);

The problem is the output of P0_5 ~ 3.2V. And the measured value is not correct. Any config is wrong?

Thanks in advance.