This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538-CC2592EM-RD: CC2538+CC2592 Custom Board does not transmit with modified sampleswitch code.

Part Number: CC2538-CC2592EM-RD
Other Parts Discussed in Thread: CC2538, CC2592, Z-STACK, CC2531, CC2530, CC2530EM

 I am using cc2538 and cc2592 on a custom designed board to transmit data to a zigbee node (whose mac address is hardcoded in the application code).

The hardware is tested by using SmartRFStudio 7 and configuring the device to use cc2592 as range extender. Tx power is set to 22dbm and it transmits well during the test. The range was found to be 10 mtrs LOS and 7 mtrs non-LOS. 

When I run the application code, the device seems to set in receive high gain mode with PC2-LNA_EN=High, PC3-PA_EN=Low and HGM(PD6 in our design,configured in code)=HIGH.

When I send something(from mobile phone to a wifi-uart bridge(connected to uart of cc2532)), it is correctly received at the CC2538, but not sent from CC2538 to destination. If someone can help, it would be great.

It is worthwhile to mention here that packet sniffer sniffs some broadcast packets coming from the 38+92 system. Sniffer does not sniff anything when i send something from mobile(that logically should transfer on zigbee radio).

Please Help.