This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1350 LP as SLIP radio for 2.4 GHz

Other Parts Discussed in Thread: CC1350, CC2650, CC1310

Hi,

Is CC1350 LP supported as SLIP radio for 2.4Ghz on Contiki?

If yes, what are the build options for SLIP radio on CC1350 Launchpad platform?

What are the build options for CC1350 SensorTag for 2.4GHz as mote?

according to github.com/.../srf06-cc26xx  it is not, correct?

Other options for the BOARD make variable are:

  • Srf06+CC26xxEM: Set BOARD=srf06/cc26xx
  • Srf06+CC13xxEM: Set BOARD=srf06/cc13xx
  • CC2650 tag: Set BOARD=sensortag/cc2650
  • CC2650 Launchpad: Set BOARD=launchpad/cc2650
  • CC1310 Launchpad: Set BOARD=launchpad/cc1310

Jan