This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SMARTRF06EBK: Dead SmartRF05EB, cannot flash bootloader.

Part Number: SMARTRF06EBK
Other Parts Discussed in Thread: CC2530EM

Hello,

I have a SmartRF05EB with a CC2530EM, I was programming it through USB and everything worked fine.

I decided to connect a CC Debugger to it and program through the CC Debugger and it worked. But now the board won't start, it won't be recognized via USB, and not even the CC Debugger will recognize it. Not even without the EM.

I think I might have overwritten the bootloader. I tried joining pin 17 and 19 to see if the bootloader was working but nothing.

Now I try to flash the bootloader using SmartRF Flash Programmer but the board is not even recognized by the CC Debugger (i.e. I get a red light on the debugger).

Is it gone for good?

Thank you.