Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK
In 07-5123-06-zigbee-cluster-library-specification, 3.13 RSSI Location, there specify commands received and generated as follows:
Commands Received
0x00 Set Absolute Location M
0x01 Set Device Configuration M
0x02 Get Device Configuration M
0x03 Get Location Data M
0x04 RSSI Response O
0x05 Send Pings O
0x06 Anchor Node Announce O
Commands Generated
0x00 Device configuration response M
0x01 Location data response M
0x02 Location data notification M
0x03 Compact location data notification M
0x04 RSSI Ping M
0x05 RSSI Request O
0x06 Report RSSI Measurements O
0x07 Request Own Location O
However, the TI Z-Stack (3.0) only includes the commands marked as mandatory (M) while the one marked as optional (O) are not included. May I ask the TI’s development team that whether those optional commands will be included in the next update of the Z-Stack or not?
If it is no plan to update, I cannot implementation the application as shown in the following figure as some commands are missing.
Thank you very much.
Best regards,
Barry