This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2630: CC2630 Errata August 2016

Part Number: CC2630


Hi

I've seen in the Errata August 2016) that the CC2630 internal 32kHz oscillator doesn't work.

But I need the CC2630 internal 32kHz oscillator.

Is the CC2630F128RHB now (Jan 2017) available with working internal oscillator? Which revision?

  • Hi Michael,

    Revision D (PG2.3) or newer devices have corrected this problem. You can find which version of the chip you have on an existing board with Flash Programmer 2. After connecting a board, click on the chip at the top left and the chip revision will be listed at the bottom left. This chip revision number corresponds to the PG number.