Other Parts Discussed in Thread: REMOTI, CC2530
I have see RemoTI but still not work.
void inittimerIR(void)
{
// CLKCONCMD &= ~0x38;;
// CLKCONCMD |= 0x18;
//Inittimer1();
//Inittimer3();
T1CTL = 0x00;
T1CCTL0 = 0x10 | 0x04;
T1CCTL1 = 0x18 | 0x04;
//T1CNTL = 0;
// T1CC0 = 85;
// T1CC1=21;
T1CC0L = 2;
T1CC0H = 0;
T1CC1L = 1;
T1CC1H = 0;
T1CNTL = 0;
T1CTL = 0x00 | 0x02;
// Wait till the single bit is cleared
while (T1CNTL == 0);
// Stop timer 1
//T1CTL = 0x00;
//timer3
//T3CTL = 0x04;
T3CTL = 0x40 | 0x02; // 4
T3CCTL0 = 0x10 | 0x04;
T3CCTL1 = 0x18 | 0x04;
// T3CC0 = 0xD2; //211
// T3CC1 = 0x46; //105
T3CC0 = 0xD2; //
T3CC1 = 0x46; //
//IRCTL |= 1;
}
void SendIRsignal(void)
{
IRCTL |= 1;
writeI2C(IRdata,IRdataLen);
IRCTL |= 0;
}