Hello,
in order to measure certain characteristics of the chip I need to enable the RF-Test mode via ZNP serial command by the host. As far as I understood what I need to do is:
Write in the NV_ITEM 0x0F07 4 bytes of parameters (mode, channel, power, test tone) and then do a soft reset. The device should now be in RF-Test mode as specified until a hard reset. But for some reason this doesnt seem to happen?
So how do I enable the RF-Test mode for the CC2538 ZNP firmware?
regards,
Thomas