Hello,
I'm looking to reduce the costs and risks of testing a radio enabled product for the CE market only. I would like to use IEEE 108.15.4 over 6LowPan
So, I would like to use the CC2538 IC only.
1) Apparently there is some Zigbee certification on this one. Does the "Zigbee certification" is only the software stack certification from the Zigbee consortium or does it include all the intentional emissions testing and compliance with CE? If the later, considering that the MCU has a different processor and stack for packet handeling, can I use the Zigbee certification to show the intentional emissions compliance for the IEEE 108.15.4 and 6LowPan ?
2) Considering that the IC is IEEE 108.15.4, have TI done some test about the intentional emissions testing from the CE norm that I could base my documents on in order to reduce the amounts of tests needed ?
Thank you very much