I use the ZTOOL tool, the device will indicates the ZDO End Device Announce.How can I reject it into the network.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I use the ZTOOL tool, the device will indicates the ZDO End Device Announce.How can I reject it into the network.
Hi user4595853
The new zstack 3.0 provides the install code functionality defined in the base device behavior specification. Basically an install code is a user defined character chain used to derive the link key and is associated to the IEEE address of the device that will join with that install code.
Look at the section 10.1 and just ask if you need more information about this, I hope this helps.
Regards,