hi all,
when i run znp at my custom board(AM3358+CC2538+cc2592)
it have some error, about OTA server**1
"
Could not register OTA endpoint with zstackserver **2
"
i try to disable OTA server, but it also some error with NWK_MGR/MAIN(Registering ZDO Callbacks Failed)
how can i open the debug log with zigbeeHA
**1:
root@arm:~/servers# ./zigbeeHAgw bbb
running zigbeegw.scr on an ARM
resetting beaglebone black
sleeping 6 seconds after reset... Using serial port: /dev/ttyO5
Received System version.
Transport Protocol Version: 2
Product ID: 0
Software Release: 2.6.3
Software Revision: 0
(Revision not specified)
done
Starting the ZigBee gateway subsystem
deviceKey = 0 (0 )
devPath = '/dev/ttyO5'
logPath = './NpiLnxLog.txt'
... freeing memory (ret 0)
Port: 2533
Following IP addresses are available:
IPv4: interface: lo IP Address 127.0.0.1
IPv4: interface: eth0 IP Address 192.168.159.148
The socket will listen on the following IP addresses:
IPv4: 0.0.0.0
IPv6: ::
0.0.0.0 means it will listen to all available IP address
waiting for first connection on #3...
NPI started (pid 2261) at Mon Feb 6 14:09:27 CST 2017
Connected to #5.(127.0.0.1 / ::a741:f2b6:e865:e4b6)
ZLSZNP started (pid 2268) at Mon Feb 6 14:09:31 CST 2017
[NWK_MGR/MAIN] : there are 2 args
[NWK_MGR/MAIN] : argv[0] = ./NWKMGR_SRVR_arm
[NWK_MGR/MAIN] : argv[1] = 127.0.0.1:2536
[NWK_MGR/MAIN] : ************************************************
[NWK_MGR/MAIN] : * Network Manager Server v1.0.1 *
[NWK_MGR/MAIN] : * The following are the avaible key commands: *
[NWK_MGR/MAIN] : * Exit Program. - q *
[NWK_MGR/MAIN] : ************************************************
NETWORK MANAGER started (pid 2276) at Mon Feb 6 14:09:32 CST 2017
[GATEWAY/MAIN] :
[GATEWAY/MAIN] : ************************************************
[GATEWAY/MAIN] : * Gateway Server v1.0.1 *
[GATEWAY/MAIN] : * The following are the avaible key commands: *
[GATEWAY/MAIN] : * Exit Program. - q *
[GATEWAY/MAIN] : ************************************************
GATEWAY SERVER started (pid 2284) at Mon Feb 6 14:09:34 CST 2017
[OTASRVR/MAIN] :
[OTASRVR/MAIN] : ************************************************
[OTASRVR/MAIN] : * OTA Upgrade Server 1.0.1 *
[OTASRVR/MAIN] : * The following are the avaible key commands: *
[OTASRVR/MAIN] : * Exit Program. - q *
[OTASRVR/MAIN] : ************************************************
[NWK_MGR/MAIN] ERROR: Endpoint Registration Failed
[NWK_MGR/MAIN] ERROR: Registering ZDO Callbacks Failed
[NWK_MGR/MAIN] ERROR: Reading Local Network Information Failed
[NWK_MGR/MAIN] : Initialization failed. Quitting now. mhoyt
OTA SERVER started (pid 2294) at Mon Feb 6 14:09:36 CST 2017
[OTASRVR/MAIN] :
Error - Could not register OTA endpoint with zstackserver.Exiting...
starting tracker with our pid ./zigbeeHAgw and pid list 2261 2268 2284 2294
===================================================
NETWORK MANAGER exited with code 255 at Mon Feb 6 14:09:36 CST 2017
./zigbeeHAgw: line 482: 2308 Killed ./track_servers $$ "$pids"
./zigbeeHAgw: line 610: killall: command not found
send: Connection reset by peer
[GATEWAY/MAIN] : Initialization failed. Quitting now.
./zigbeeHAgw: line 627: killall: command not found
**2:
NWK_MGR/MAIN] ERROR: Endpoint Registration Failed
[NWK_MGR/MAIN] ERROR: Registering ZDO Callbacks Failed
[NWK_MGR/MAIN] ERROR: Reading Local Network Information Failed
[NWK_MGR/MAIN] : Initialization failed. Quitting now. mhoyt
**3:
ewarm
FEATURE_SYSTEM_STATS
xPOWER_SAVING
CC2538_USE_ALTERNATE_INTERRUPT_MAP=1
CC2538ZNP
FEATURE_RESET_MACRO
ASSERT_RESET
FAKE_CRC_SHDW
ZDNWKMGR_MIN_TRANSMISSIONS=0
xHAL_SPI=TRUE
ZNP_ALT
MT_UART_DEFAULT_OVERFLOW=FALSE
xHAL_UART_USB
xUSB_SETUP_MAX_NUMBER_OF_INTERFACES=5
TC_LINKKEY_JOIN
HAL_UART=TRUE
MT_ZDO_MGMT
MT_ZDO_EXTENSIONS
PA_LNA_CC2592
HAL_PA_LNA
OSC32K_CRYSTAL_INSTALLED
MT_ZDO_CB_FUNC
MT_ZDO_FUNC