Part Number: CC2650EMK
Other Parts Discussed in Thread: SMARTRF06EBK, CC2650
Hi All,
I want to power the CC2650EMK as a standalone device (without SmartRF06EBK) and I have the some questions:
1. In the CC2650EMK Quick Start Guide (http://www.ti.com/lit/pdf/swru403 ), the SmartRF external power supply requirements are:
Nominal voltage: 2.1 to 3.3 VDC
Maximum voltage 3.6 VDC
Max Current: 1000 mA
Efficiency Level V
Are these requirements the same when I power the EM alone without the SmartRF?
2. How do I know the VDD and GND pins in the EM? I found a pin-out table in the SmartRF06 User's Guide (http://www.ti.com/lit/pdf/swru321) section 6.10, it has 4 GND pins, 2 VDD1 pins and one VDD2 pin. Which pins should I use?
Thanks in advance!