This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2630: Analog comparator

Part Number: CC2630

Hallo,

is it possible to use the analog comparator of the CC2630 to compare an input voltage from a load cell sensor to a predefined threshold and trigger an interrupt if the threshold is exceed? Are there any examples of how to configure the pins, the comparator and the interrupt? I assume that when the CC2630 is woken by the interrupt, we can determine the source of the interrupt, i.e. interrupt from comparator vs. interrupt from key. Correct?

Thanks in advance,

Todor