This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650EM-5XD-RD: Compatible with SmartRF05EB

Part Number: CC2650EM-5XD-RD
Other Parts Discussed in Thread: CC2650MODA, LAUNCHXL-CC2650, Z-STACK

Is the CC2650EM-5XD-RD module compatible with the SmartRF05EB?  It looks like the CC2650DK ships with the SmartFR06EB but since we already have two of the '05 boards I want to know if we can just order the CC2650EM-5XD-RD modules.

The overall goal is to have a development environment for creating a ZNP+ZAP device.  There would be one battery powered End Point and one mains powered Coordinator.  The actual device used would be a CC2650MODA module with a small Cortex-M3 on the coordinator side and a CC2650MODA module with a Cortex-M7 on the End Point side.

The CC2650MODA-EXP432P401R might be an alternative if this eval board set is able to program the CC2650MODA module.