This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538EMK: CC2538 as ZNP (UART Communication)

Part Number: CC2538EMK
Other Parts Discussed in Thread: CC2538, Z-STACK,

Hello,

I am working on CC2538 .

We are planning to use CC2538 as ZNP.

1) If I use CC2538 as ZNP ,can i use its other peripherals for some other application?

for example: One UART is used for serial communication between other Micro controller(HOST MC) .There is One more UART  left which can be used for some other purpose .can it be used?

2) Our Application need one CC2538 to act as COORDINATOR and like wise there will many other CC2538's  which will act as ROUTERS .

Now the communication occurs on the air, that is the data transmitted  by the COORDINATOR is received by the ROUTER.where will it be received ?Can it be seen in PC using serial terminals if the ROUTER is connected to PC?

Note :We don't have SmartRF06 board to use SmartRF Studio.(XDS100v3 debugger is used for flashing and debugging)

How can it be monitored using some other tool?

For your reference our Application Block diagram is below: