Part Number: CC2650
Other Parts Discussed in Thread: CC2630, CC2530, CC2538, Z-STACK
Hi all,
I'm an experienced embedded developer with plenty of 8/32 bit MCUs and many kinds of communication modules. I have been asked to do some research on possible solutions for the following system description:
1. The system will include 20-100 standalone microwave radar sensors for human movement detection. Standalone meaning that each sensor will be battery powered and have an MCU and a transciever. Each mA matters .
2. The sensors need to be sampled at minimum of 3/4Hz, preferably constantly sampling. Upon detection of trigger event (voltage level drop), the mcu should transmit its' ID to central node/modem for further processing.
3. The sensors will be spread in large outdoor areas with maximum of 30 meters between closest units. The placement procedure is to be as simple as possible (just turning a switch on or something like that), avoiding the use of repeaters and such. Think of it as a sensors mine field.
A few questions:
1. From the information I gathered so far I think that the CC2650/30 is the best suit for this purpose. Is that a correct assumption?
2. Using the Zigbee protocol with the mesh networking setup sounds like exactly what I need, as the distances between nodes and the data rate is very low.
3. I am not familiar with the depths of the Zigbee protocol and have no experience with the CC2xxx family. I have seen that there are different versions of ZStack and different supports for the mesh networking on the CC2xxx. Im also not familiar with the terms used for Zstack/Zigbee (ZAP/ZAR/ZC/ZP etc.).
4. Can you please point me in the direction of the correct layout, version and documantation sources for the rigth MCU/ZStack and any other recommendations you have
Thank you very much in advance,
Roman Ivnitzki