Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK, , CC2531EMK, CC2650, CC2538, CC2630, CC2590
Tool/software: Linux
Hello people
We are in need of a development kit which can help us in this project to develop a embedded linux board which can communicate with a zigbee module through UART(or I2C/SPI) to send zigbee commands to other zigbee end devices. We need linux gateway source code/application/driver and its reference design and reference designs of other zigbee end devices. The linux development board right now has only USB port but eventually we will be communicating with serial interface. Does the CC2530 kit have USB zigbee controller which can be programmed as a zigbee coordinator also if we can also program it with our development board. Please provide me with a solution to develop such a environment. Thank you.