Part Number: CC2538EMK
Other Parts Discussed in Thread: CC2538
Greetings,
I tried to run the SSI (SPI master) example in CC2538 Foundation Firmware (located in : swrc271a.zip\cc2538_foundation_firmware_1_0_1_0\driverlib\cc2538\examples\ssi) but it did not work properly. Nothing appears on the LCD of SmartRF06.
The same happened when I tried to run the UART example, nothing on the LCD!
The LCD runs fine when I load the PER test, so it must be a code problem.
Any ideas?
Regards
* James *