This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538: Zigbeee custom board with CC2592

Part Number: CC2538
Other Parts Discussed in Thread: CC2592, CC2531,

Hi TI,

I'm trying to investigate the custom board I have with CC2538 with CC2592 range extender. I'm using the latest ubiqua software and official CC2531 hardware sniffer.

My test setup is:

1.) I set the TX POWER to 20dBm

2.) Set up the sniffer(CC2531) and coordinator (custom board CC2538 + CC2592) roughly 5cm away from each other

2.) Set the coordinator  to send 1 broadcast (around 10 dummy bytes zigbee payload)

3.) Checked the sniffer

Here's the reading I got for RSSI:

Is this supposed to be like this? or closer to 20dBm value? How do I test if the antenna of my board doesn't have any issue?

Thank you.