HI,
In ZSTACK,I find that, the cpu(cc2530) doesn't execute external IO interrupt in time.
I just want , the cpu detects the external I/O interrupt (the Generation time of the interrupt is about 20ms one time), then a pin of the cpu outputs high voltage in time, but i find that the output of the pin is slower than the interrupt generated about>15ms,and the time is defferent every time , why?what should i do reduce the deviation to 2ms?
thanks!