This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530 ZStack 3.0

Part Number: CC2530DK
Other Parts Discussed in Thread: CC2530, Z-STACK

I have TI CC2530 Zigbee Development Kit. Here are the below steps for the debug the Sample application ZStack 3.0 code ie. Sample Light.

1. In IAR Workbench I did Rebuild All and Download and Debug, so one of my device is configured as the coordinator.

2. Second I selected as End Device in IAR workbench and Download and Debug to another device as End Device. 

3. From TI Zigbee Development board, in LCD I set PAN ID as EFFF on both board.

4. On the both board the I pressed <APP MENU> to  <TOGGLE LIGHT>. BUT it works only on individual board. So, Is network not created ? 

5. As per the User Manual, 

"Press OK again multiple times on the <TOGGLE LIGHT> Screen on End Device
Notice that LED1 is turning on and off"

This is not working in my case.

 What is the problem ? 

If I want to make my customize code for my application, what are the changes in Sample Application ZStack 3.0 ?