Tool/software: Linux
Hi,
We're performing radio immunity testing against our board, based on the CC2520 reference design, by setting up a Linux 6lowpan network between two devices. When we reach 633MHz the module under test stops receiving data but can still send. This has been verified by looking at the rx/tx bytes counters in the Linux system on both ends. The RSSI register is 0xE3 when this happens.
Do you have any idea on what could cause this behaviour? Is there any register on the CC2520 that could help us determine what is happening?
Thanks,
// Måns