Other Parts Discussed in Thread: CC2530, Z-STACK
We have a product using the CC2530.The SPI interface of CC2530 connection external FLASH. CC2530 is the SPI master. Use USART1 the alternative1. Hardware connections are as follows. Test found that there is no clock signal output P0.3. When modified to use USART0 of the alternative1, test P0.5, The CC2530 have clock output. Why? If the special requirements of IC, Why did not the notation description in the specification?