Part Number: CC2538
Other Parts Discussed in Thread: TIMAC
Hi Support,
Am using TIMAC and the CC2538 is setup in a beacon enabled network where there is a PAN coordinator and several “routers”.
The router is setup with both Coordinator and Device function.
Issue #1:
When the router device try to send data to the its parent router, the data is sending out during the its own beacon time instead of the parent beacon time.
Since the data would not be ACK by the parent router when it sending out, the data will be sending again when the next parent beacon.
This has create unnecessary data transmission for the router.
Please refer to the attached screenshot of the sniffer log.
Issue #2:
When the CC2538 is heated to around 70-80 degree Celcius, the device does not send out any beacon anymore.
However, the device is still able to sync with its parent router and sending out data when requested by the parent router.
This means the other network activities is still working correctly except sending out its own beacon.
When the heat is removed, the router will be able to send out its beacon again with the same timing previously and continue the sequence number from where it stop previously.
Please advise.
Thanks.