This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I debug the CC2530 SerialApp. the uart link the computer USB port through FTDI chip, I send the 15 bytes data mutually in the interval of 50ms, but data stop after random time.normally ten minutes. I found the prgram don't go into the UART callback function, it seem to that the uart DMA function have the bug. any propose is appreciated.
Is this issue solved?
I also have similar problem.
Situations are below;
1. Using two CC2530EMs on CC2530EBs.
2.EBs are connected to PC via RS232C.
3.Run 'SerialApp' on CC2530EMs.(Coordinator and Router)
4.Connection with ZigBee was OK.
5. On PC, I run two 'Hyperterminal' for COM1(to Coordinator EB) and COM4(Router EB).
6. I typed some words on one Hyperterminal, then on another Hyperterminal there were the words I typed.
7. I transfered a file via Hyperterminal, BUT transfering was stopped during sending. After that the connection failed.
From 1 to 6, they are OK. But in situation-7, SerialApp seems to stop.
Are there some solutions? Please help.
Hi,
There is a known issue regarding the serialApp sample application:
Quoting the ZStack-CC2530 Release Notes (known issues section)
- SerialApp is not reliable when used for high-speed, large file transfers -
the receiving application occasionally drops a byte.
Hi, Igor.
You're right. I found the quote in the Release Note.
I appreciate your answer. Thank you so much.