This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530:CC2530

Part Number: CC2530


CC2530 TI tool Z - tool use.
Module burning \ Z - Stack Home 1.2.2a. 44539 \ Projects \ zstack \ ZAP \ ZNP - HexFiles \ CC2530 \ CC2530ZNP - Pro. Hex firmware。
P0.2 0.3 0.4 0.5 by serial port flow control P2.0 connect to GND。
Using z-tool debugging tools, so we have to use a few times, often NO device Found, set up 115200 n 8 1 RTS/CTS. Don't know why.
Have set when the connection is successful, after all, there should be NO wrong, directly connect a serial port tool is to be able to identify the serial port, ztool inside also identify a serial port, but the connection when the tip “NO device Found”.
What it's worth noting that place? Or a detailed manual.My major is in accordance with the zstack manual operation。