This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2350



I doing tests on rc2400hp module cc2350 znp processor

the following are the issues I am facing this. I am using api mode for data transfer

1. Failed to get expected routing table response (ZDO_MGMT_RTG_RSP) from the coordinator for ZDO_MGMT_RTG_REQ.  
2. While transmitting 6 different broadcast packets (with packet size 94 bytes) at a time, unknown response from the coordinator (Status return value : 0x1A).
3. While transmitting more than 1 packet in unicast (with packet size 94 byte) at a time, SRSP and ZB_SEND_DATA_CONFIRM are received unevenly, which are not equal to the no.of packets being transmitted. 
4.how to disable the nwk layer security key so that I can send 99 bytes payload