Part Number: CC2530
Hi,
My SmartRF05 1.8.1 board is not detecting the CC2530EM 1.6, The USB LED D6 in the Smart RF board is not detecting and voltage across the LED is 3.3V on either sides of the LED, it is not going low as I am not able to program the board. Also the LCD display in the Smart RF EM shows that the EM(CC2530) is not detected.
Please tell which part of the board has fault so as to debug and make board working.
Thanks & Regards
Krishna