Part Number: CC2531
Hi,
I am trying to run ZNP on a CC2531 USB dongle without success.
What I have done so far is:
1. Loaded CC2531SB.hex to the dongle.
2. Compiled znp CC2531-ProdSBL.
3. Run sim2bin on the CC2531.sim file that came out from the step above, creating CC2531.bin
4. Used SerialBootTool to upload CC2531.bin
All above steps worked fine.
The problem is that after that I can connect to the serial port only during the first minute, while the dongle is still running the bootloader. After the first minute I can still see the serial port on the devices manger, but I cannot connect to it. It seems like there is something wrong with the znp app or that it is not starting.
Any ideas to help me?
Thanks,
Rodrigo F