This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Recently,I am studying the z-stack 1.4.3-1.2.1.Now I want to add an UART application to my project.When I read the source of SerialApp.c.I don't understand the difference between the two functions:rxCB_Loopback( uint8 port, uint8 event ) and rxCB( uint8 port, uint8 event ).
In adddition,I have another question:I have create a SimpleApp application .Should I add another Task for UART,and I just need the UART to transmit the imformation.I really expect someone could tell me that.Thank you
Hi,
The method rxCB_Loopback is used to write out on UART the same data as was received on UART. This is just used for testing, and is enabled if you define SERIAL_APP_LOOPBACK.
The RxCB() is default method to use. This method will send the data that was received on UART out on the air.
Regards,
Bjørn