Hi,
I have been working for some time now with 6lbr. My setup is basically a RPI2 which acts as a border router and in which 6lbr is deployed. The RPI2 has connected to one of its USB ports a CC2650 sensortag in which a slip-radio program has been flashed. The RPI2 will then communicate with other sensors through this 6LowPAN network deployed.
My issue comes when I want to replace my slip-radio with the following OpenLabs module: http://openlabs.co/store/Raspberry-Pi-802.15.4-radio . I have succesfully created a network interface and managed to ping two RPI2's through this module and interface, however I can't get to ping a Rapsberry Pi 2 with a sensortag which runs the cc26xx-web-demo.
I want to run the 6lbr application with the openlabs module and substitute the slip-radio in order to solve this issue. Since the slip-radio+6lbr is operational the open-labs+6lbr should also work however for this approach there are many open issues over the internet and none of them have come to a specific solution. Has anybody achieved or at least know any approaches to achieve this compatibility?
Thank you very much and I hope the description above is clear.