This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650STK: Disconnect from 6lbr after a while or clicking the "web" button

Part Number: CC2650STK

I used raspberry pi with rasbian 4.1 running 6lbr whose version was 1.3.3. And i used nullRDC on cc2650stk. At fist, i can access the [bbbb::100]/sensors.html and the graph of the two sensortags is perfect. But after a while wheni clicked the "web", randomly one sensortag would be disconnected. Just like the screenshot below. And then i switched to Beaglebone whose 6lbr version was also 1.3.3 and the same disconnection problem occurred.