This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/CC2530: Use IAR and Flash Programming to setup a Zigbee Network

Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK,

Tool/software: TI C/C++ Compiler

Hi,
I'm having an issue now. I want to build a simple Zigbee Network using two CC2530 nodes. I don't have EB like smartRF05EB. I'm just using CC Debugger to flash the Coordinator and EndDevice hex file from the GenericApp sample application but I still don't know how to see the packet capturing between them and I don't know if it is in a network yet. I read a guide using Z-Tool and Z-Stack to set up the network but my Z-Tool won't recognize my CC2530 so I have to find another way.
One small question is that I do have to power up both CC2530 to transmit and receive packets right? So if I plug my coordinator which transmits packets into my computer through CCDebugger and the EndDevice I power it up with another source then is it OK?

Things I'm using:

1. CCDebugger
2. CC2530

Tools I'm using

1. Z-Stack 3.0.0

2. IAR Workbench for 8051
3. TI Flash Programmer

I'm looking forward to responses. Thank you guys so much and I'm appreciated.