Part Number: CC2530
Other Parts Discussed in Thread: CC2541, CC2533, REMOTI
Which pins of CC2530 should use for I2C interface??
Please reply instantly because of emergency.......
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
It seems I2C is available in CC2533 and CC2541 only.
On the CC2533 and CC2541, the I2C module is connected to pins 2 and 3 and uses the P2 interrupt to the
CPU. Pins 2 and 3 can alternatively be controlled as two GPIO pins if they are not used by the I2C module.
Please refer to section - I2C of CC253x User Guide (SWRU191) for further details.
2-Wire debug is available in CC253x devices.
The two-wire debug interface allows programming of the on-chip flash, and it provides access to memory
and register contents and debug features such as breakpoints, single-stepping, and register modification.
The debug interface uses I/O pins P2.1 and P2.2 as debug data and debug clock, respectively, during
debug mode. These I/O pins can be used as general-purpose I/O only while the device is not in debug
mode. Thus, the debug interface does not interfere with any peripheral I/O pins.
Please refer to section - Debug Interface of CC253x User Guide (SWRU191) for further details.
Thanks,
PM