Part Number: CC2531
Other Parts Discussed in Thread: Z-STACK
Hello,
I'm trying to join a router to a coordinator with secure active.
But I'm facing a problem that when router connects, after some time it is kicked from the network.
At coordinator side, I can see that it's giving timeout for this node. The code that is doing this is:
if(tempJoiningDescNode->NodeJoinTimeout == 0)
{
//Check if the key exchange is required
if(bdbAttributes.bdbTrustCenterRequireKeyExchange)
{
AddrMgrEntry_t entry;
entry.user = ADDRMGR_USER_DEFAULT;
osal_memcpy(entry.extAddr,tempJoiningDescNode->bdbJoiningNodeEui64, Z_EXTADDR_LEN);
if(AddrMgrEntryLookupExt(&entry))
{
ZDSecMgrAPSRemove(entry.nwkAddr,entry.extAddr,tempJoiningDescNode->parentAddr);
}
}
Variable bdbTrustCenterRequireKeyExchange is set to true. The consequence of this is that coordinator is sending a leave request.
Should I set some variable on router side so it can exchange the key?
I tested one of your examples (samplelight and sampleswitch) with a coordinator and end device, and it works properly.
My code base for developing is yours GeneraApp project.
I'm using Z-stack 3.0
Thanks in advance.
BR,
Igor