This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: PICTL and PADSC

Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK,

Hi,

1. According to page 79 of http://www.ti.com/lit/ug/swru191f/swru191f.pdf, it says that I need to set PICTL and PADSC to 1 when the CC2530 drops below 2.6v. Is there a function in Z-Stack that can automatically do this, or do I have to do this myself? If I have to do it myself, how would I do this correctly?

2. Also, are there other changes in the code that I should do in order to keep the CC2530 working properly and without problems when the voltage is below 2.6v? (In other words, maximizing performance of the CC2530 when below 2.6v)